Search FAQs
What is the thickness of the Steel sheet metal of Blokset Panel.
The Steel sheet metal thickness used in Blokset Panel is as per the below table:
Blokset Steel sheet metal thickness
Housing | Thickness mm |
Door | 2.00mm |
Rear panels | 2.00mm |
Side panels | 2.00mm |
Roof/Top | 2.00mm |
Frame | 2.00mm |
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: