Search FAQs
Is the Modbus port on a Unity Momentum considered Modbus Port 1 when using an XMIT instruction ?
Issue
What are the Modbus port designations on a Unity Momentum M1 and M1E
Product Line
Unity Momentum, Unity Pro
Resolution
When using a Unity Momentum M1, the Modbus ports are designated as MB port 0 and MB port 1.
When using a Unity Momentum M1E, the Modbus port is designated as MB port 0.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: