{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where can I find the FO (Factory Order) or Q2C number for an M-Flex drive?
Issue:
Need to identify the Factory Order, or Quote to Cash number for an enclosed M-Flex drive.

Product Line:
Enclosed Altivar 61, Enclosed Altivar 71, Enclosed ATV61, Enclosed ATV71, M-Flex, Mflex

Environment:
All models

Cause:
To determine warranty status or check the Bill of Materials for spare parts.

Resolution:
One the back of the M-Flex enclosure door of the is the nameplate. At the bottom right is a box with the Factory Order number (Q2C number).  The Field Wiring Diagram number should be a similar number.

Schneider Electric Nigeria

Attachment(s)
M-Flex nameplate.jpg [129.58 KB]