undefined undefined
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Powerlogic Scada Expert (PSE) Runtime Manager hangs on startup.
Issue:
When Runtime Manager is started it will hang up and only say that it is not responding, all server processes will not use any additional CPU.

Product Line:
Powerlogic Scada Expert version 7.40, 7.30, 7.20

Cause:
This has been seen on systems with multiple CPU's and they are set to use "ALL" for each process when running the 'Computer Setup Wizard'.

Resolution:
Modify the CPU that each process uses from "ALL" to a set CPU from the Computer Setup Wizard.  Once this is done the runtime project will start as normal.

Schneider Electric Nigeria