{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
KVM1116P, KVM2116P, and KVM2132P KVM Switches using standalone WinClient and Java Client - Compatibility/Video Issue

Issue

When using the WinClient or Java Client with my KVM1116P, KVM2116P or KVM2132P IP KVM Switch, why is my video distorted (as seen below)?





Product Line
  • KVM Switches
    • KVM1116P SMB IP KVM
    • KVM2116P Enterprise IP KVM
    • KVM2132P Enterprise IP KVM



Environment
  • Users utilizing the standalone WinClient or Java Client downloaded from the KVM Switch to access devices remotely
  • Users possibly in environments with both SMB and Enterprise KVMs

Cause

This can be caused by using the WinClient (WinClient.exe) or Java Client (JavaClient.jar) being downloaded from an SMB KVM being used with an Enterprise KVM, or vice versa. Each SMB or Enterprise KVM must be used with the respective client or else the video problem above may be experienced.

Also, for the Java Client, having multiple versions of Java installed on the computer you are using the Java Client on could contribute to this problem.



Resolution

For each type of KVM, make sure to download the WinClient or Java Client directly from the appropriate KVM. If you have done that and are using the Java Client, verify if multiple versions of Java are installed on the machine. If possible, try to remove all but a supported version (most Java 6 and Java 7 versions are designed to work).


Schneider Electric Nigeria

KVM1116P, KVM2116P, and KVM2132P KVM Switches using standalone WinClient and Java Client - Compatibility/Video Issue

Issue

When using the WinClient or Java Client with my KVM1116P, KVM2116P or KVM2132P IP KVM Switch, why is my video distorted (as seen below)?





Product Line
  • KVM Switches
    • KVM1116P SMB IP KVM
    • KVM2116P Enterprise IP KVM
    • KVM2132P Enterprise IP KVM



Environment
  • Users utilizing the standalone WinClient or Java Client downloaded from the KVM Switch to access devices remotely
  • Users possibly in environments with both SMB and Enterprise KVMs

Cause

This can be caused by using the WinClient (WinClient.exe) or Java Client (JavaClient.jar) being downloaded from an SMB KVM being used with an Enterprise KVM, or vice versa. Each SMB or Enterprise KVM must be used with the respective client or else the video problem above may be experienced.

Also, for the Java Client, having multiple versions of Java installed on the computer you are using the Java Client on could contribute to this problem.



Resolution

For each type of KVM, make sure to download the WinClient or Java Client directly from the appropriate KVM. If you have done that and are using the Java Client, verify if multiple versions of Java are installed on the machine. If possible, try to remove all but a supported version (most Java 6 and Java 7 versions are designed to work).


Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
move-arrow-top