Issue:
ATV312 Communication Protocols
Product line:
Altivar 312
Environment:
All range All serial number
Cause:
ATV312 Communication Protocols
Product line:
Altivar 312
Environment:
All range All serial number
Cause:
Ethernet TCP/IP
Resolution:
The communication protocol card that are available on the ATV312 are:
Resolution:
The communication protocol card that are available on the ATV312 are:
Modbus – Standard on the ATV312
CanOpen – Standard on the ATV312
Profibus – Option VW3A31207
CanOpen Daisy Chain - – Option VW3A31208
DeviceNet – Option VW3A31209
Early versions of the ATV312 documentation stated that Ethernet TCP/IP communication cards would become available as an option. This was incorrect. Neither Ethernet TCP/IP or Ethernet IP is currently available for this drive as an option card from Schneider Electric
Released for:Schneider Electric Nigeria