{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How do I configure my ATV312 drive for forward and reverse direction using +10/-10V speed reference?
Issue:
ATV312 configuration for forward and reverse using +10/-10V speed reference

Product Line:
Altivar 312 series drives.

Environment:
All models, All serial numbers.

Cause:
Customer needs to control the drive forward and reverse with a single run command and +10 to -10V input for speed/direction control.

Resolution:
AI2 input can be used for +10 to -10V input.   Configure parameter FR1 to AI2 under the CTL menu to have the drive look at AI2 as the primary speed reference.  Connect your +10/-10V speed reference between AI2 and COM on the drive.

Schneider Electric

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.