{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can SoMove transfer the configuration from one drive to another of the same model number, but different firmware versions?

Issue:
Transfer programming from one drive to another using SoMove.

Product Line:
Altivar Variable Frequency Drives

Environment:
All models compatible with SoMove.

Cause:
None

Resolution:
It is possible to transfer a configuration from one drive to another drive of the same model, but different firmware versions.  However, there may be problems if going from a newer firmware level to an older firmware level if the new has additional parameters or if the new firmware includes a physical hardware update like a new micro processor.

Schneider Electric Nigeria