undefined [object Object]
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Is it possible to delete the buffer contents or events in the BMXNOR0200 module configured as Server in IEC Protocol, when the communication between the server and client is not present.
Issue: The customer wants to delete the buffer of BMXNOR0200

Product Line: BMXNOR0200 V1.6 & V1.7

Environment: Unity Pro V12 installed on Windows 7 Pro

Resolution:

It is not possible to delete the buffer contents or events in the BMXNOR0200. When the module configured as Server in IEC Protocol and the communication between the server and client is not present.

Schneider Electric Nigeria

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.