{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What device types are natively supported and compatible in ION Setup 3.1?

Article available in these languages: Spanish

Issue
A list of devices supported and / or compatible in the most recent version of ION Setup 3.1.

Product Line
ION Setup Version:  3.1.19192.03

Environment
Supported Device types and compatibility with ION Setup software

Cause
The posted ION Setup user manual is not updated as frequently as new software versions are released. The manual states that "The devices supported by ION Setup are subject to change".

Resolution
UPDATED 8/8/19
The list below indicates devices that are currently supported in the latest version of ION Setup. Definitions of abbreviations and acronyms can be found further below.

Please note that many devices listed here have very limited functionality in ION Setup and are only present for troubleshooting or commissioning purposes.
Schneider Electric / Square D / Power Measurement BrandsSiemensOther
Conzerv EM1200 Series Energy MeterSiemens 4300 Power MeterAB 1400 PB Power Meter
Conzerv EM6400 Series Load ManagerSiemens 4700 Power MeterAB 1400 PD Power Meter
Conzerv EM6400H Series Load ManagerSiemens 4720 Power MeterModbus RTU Device
Conzerv EM6400NG Series Load ManagerSiemens 9200 Power MeterModbus TCP Device
EasyLogic DM6000 Series Digital MeterSiemens 9300 Power Meter
EasyLogic DM6000H Series Power MeterSiemens 9330 Power Meter
EasyLogic EM1000 Series Energy MeterSiemens 9340 Power Meter
EasyLogic PM1000 Series Power MeterSiemens 9350 Power Meter
EasyLogic PM1000H Series Power MeterSiemens 9360 Power Meter
EasyLogic PM2000 Series Power MeterSiemens 9410 Power Meter
ION6200 Power MeterSiemens 9500 Power Meter
ION6300 Power MeterSiemens 9500 RTU
ION7300 Power MeterSiemens 9510 Power Meter
ION7330 Power MeterSiemens 9510 RTU
ION7350 Power MeterSiemens 9600 Power Meter
ION7400 Power MeterSiemens 9610 Power Meter
ION7500 Power MeterSiemens 9700 Power Meter
ION7500-RTUSiemens 9810 Power Meter
ION7550 Power Meter
ION7550-RTU
ION7600 Power Meter
ION7650 Power Meter
ION7700 Power Meter
ION8300 Power Meter
ION8400 Power Meter
ION8500 Power Meter
ION8600 Power Meter
ION8650 Power Meter
ION8800 Power Meter
ION9000 Series Power Meter
MicroLogic Circuit Breaker
MicroLogic ULP/IFE Circuit Breaker
PML 3300 ACM Power Meter
PML 3350 PDM Demand Monitor
PML 3710 ACM Power Meter
PML 3720 ACM Power Meter
PML 3750 PDC Demand Controller
PML 3800 Mini RTU
PowerLogic Branch Circuit Power Meter
PowerLogic CM2000 Series Circuit Monitor
PowerLogic CM3000 Series Circuit Monitor
PowerLogic CM4000 Series Circuit Monitor
PowerLogic E5600 Energy Meter
PowerLogic EM3500 Series Energy Meter
PowerLogic EM4200 Series Enercept Meter
PowerLogic EM4900
PowerLogic EM7000 Series Energy meter
PowerLogic Enercept Meter
PowerLogic iEM3000 Series Energy Meter
PowerLogic Model 98A Temperature Controller
PowerLogic PM3000 Series Power Meter
PowerLogic PM5000 Series Power Meter
PowerLogic PM600 Series Power Meter
PowerLogic PM700 Series Power Meter
PowerLogic PM800 Series Power Meter
PowerLogic PM8000 Power Meter
PowerLogic SEPAM Digital Relay
Vigilohm IFL Insulation Fault Locator
Vigilohm IMD Insulation Monitoring Device


List of supported Modbus RTU-based devices:
Veris BCM
Momentum PLC A8
Momentum PLC A16
Momentum PLC D10
Momentum PLC D16
Twido PLC D12
Twido PLC D28
Twido PLC D44

Abbreviations:
Mod: Modbus
RTU: Remote Terminal Unit
BCPM: Branch Circuit Power Meter
BCM: Branch Current Monitor
ULP: Universal Logic Plug
WAGES: Water Air Gas Electricity Steam
EPSS: Emergency Power Supply System
PLC: Programmable Logic Controller

To download the latest version of ION Setup software, refer to article FA212816.

Schneider Electric Nigeria