{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the service breaking capacity and what is the advantage of that on the reliability of breaker?

In a correctly designed installation, a circuit-breaker is never required to operate at its maximum breaking current (Icu). For this reason, a new characteristic has been introduced which is the rated service short-circuit breaking capacity (Ics). IEC 60947-2 expresses (Ics) as a percentage (25, 50, 75, 100%) of (Icu) .

The rated breaking capacity (Icu) or (Icn) is the maximum fault-current a circuit-breaker can successfully interrupt without being damaged. These are very high currents of extremely low probability. In normal circumstances, the fault-currents are considerably less than the (Icu) of the circuit breaker.

On the other hand, (Ics) can be considered as high currents of low probability. It is important that (Ics) be interrupted under good conditions to ensure that the circuit breaker would be immediately ready for re-closure after the faulty circuit has been repaired.

The standard test sequence is as follows: O - CO - CO (at Ics)
Tests carried out following this sequence are intended to verify that the circuit breaker is in a good state and available for normal service.
For domestic circuit breakers, Ics = k Icn where the values for the factor "k" are illustrated on table XIV in IEC 60898.
In Europe, it is an industrial practice to use a k factor of 100% so that Ics = Icu.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.