Search FAQs
What is the part number for the ATS22 remote keypad?
Issue:
What is the remote keypad for the ATS22?
Product Line:
Altistart 22 ATS22
Environment:
All models
Cause:
Keypad interface to be remote from ATS22.
Resolution:
The accessory remote keypad options are:
VW3G22101 for IP54 / Nema 12
VW3G22102 for IP65
Cable options to connect the keypad to the ATS22 are (sold separately):
VW3A1104R10 for 1 meter length
VW3A1104R30 for 3 meter length
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: