{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What does the short circuit capacity parameter shown in the VFD catalog indicate ?

The Prospective Short circuit capacity mentioned in the drive catalog indicates the drive's suitability to use in an electrical feeder without any additional input impedance to the line supply. It means, for example, the drive ATV61H075N4 can be used up to 5KA short circuit current-rated supply feeder without any problem.  If the supply feeder's SCC rating is higher than the value mentioned in the catalog, it is necessary to use a line choke or DC choke to increase the input impedance of the drive, which will help to increase the PSCC rating of the drive above 50KA to 100KA. It will also help to reduce the peak current, RMS current, and harmonics. The document in the below attachment will help to explain the effect of PSCC in drive functioning in detail.

Generally, there are two topics concerning the short-circuit capability of the mains:
a)During operation:
A strong mains supply (= high Isc) has a low impedance. Therefore it allows high peak current, RMS current and harmonic, which can overload and damage the rectifier and DC Bus capacitors of the standard drive.
With a DC choke (which is behind the rectifier) a Isc of 50kA is allowed.
With a line choke (which is in front of the rectifier) a Isc of 100kA is allowed.

b) In case of a short circuit:
If there is a short circuit the protective device (fuse or circuit breaker) must be able to interrupt this high current. If this is not the case, it will burn the drive input.

Schneider Electric Nigeria

Attachment(s)
Pages from Catalogue ATV61_EN.pdf [155.87 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: