{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can I use PID controls on an E-Flex or M-Flex that has an HOA switch?

Issue:
Trying to setup PID control on an ATV61/71 with a HOA switch.

Product Line:

ATV61/71, E-Flex, M-Flex

Environment:
All of the ATV61/71, E-Flex, M-Flex

Cause:
None

Resolution:
To allow PID control in Auto mode and manual reference control in HAND, the logic input for PID AUTO/MAN or reference 2 switch must be setup so that the contact is closed in HAND mode and open in AUTO mode.  The logic input causes the manual control to override the PID.

Schneider Electric Nigeria