Issue:
Display shows EEF
Product Line:
ATS48
Environment:
All models and serial numbers
Cause:
The EEF fault appears if there is a problem reading or writing information to EEPROM memory chips on either the control board or power board.
This fault is not stored in the fault history.
Probable Causes
• The control board is defective.
• The power board is defective.
Resolution:
Replace the control board.
Replace the power board.
Released for:Schneider Electric Nigeria