Search FAQs
What type of overload comes with the GV2, GV3 and GV7 manual starter and protector?
Issue:
GV Manual Motor Starter and Overloads' class
Product Line:
GV type Tesys manual starters.
Environment:
Tesys manual starters
Cause:
Determination of overload type furnished with the Tesys GV manul motor starters.
Resolution:
The overloads supplied with the GV2, GV3 and GV7 manual starters are Class 10, ambient compensated bimetallic.
GV Manual Motor Starter and Overloads' class
Product Line:
GV type Tesys manual starters.
Environment:
Tesys manual starters
Cause:
Determination of overload type furnished with the Tesys GV manul motor starters.
Resolution:
The overloads supplied with the GV2, GV3 and GV7 manual starters are Class 10, ambient compensated bimetallic.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: