{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Video: Resetting a LTMR Tesys T module back to factory default settings locally

Issue :
How to reset a LTMR Tesys T module back to factory default settings locally?

Product Line:
Motor control / Protection components

Environment:
LTMR
Tesys T

Cause:
Need to reset the module back to factory default settings locally to clear any user configuration.

Resolution:



1) Make sure the module is in one of the following states : Ready, Not ready or System configuration. (If the product is in Start or Run state, the return to factory setting is ignored)
2) Press and hold the Test/Reset button down for more than 15 seconds , but not exceeding 20 seconds and release it.
3) The unit will execute a reset to factory settings.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: