{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Does Somachine support ZBRN1 DTM?

Issue:
Looking for confirmation of support for ZBRN1 DTM in SoMachine

Product Line:
SoMachine

Resolution:
SoMachine v3.1 did not support the ZBRN1 DTMs. It supported only ZBRN2 which are for serial communications. The Harmony DTM is supported in SoMachine V4/V4.1 and onwards versions but not in V3.1.

The DTM can also be added to SoMachine V3.1 but it is validated for SoMachine versions > V4

(See Release notes of SoMachine)
Note: Only DTM for serial communication (ZBRN2) can be used in SoMachine V4.1 - Modbus TCP is not possible that time with SoMachine v4.1 (ZBRN1)!

Today if we check with SoMachine version v4.3, we can add ZBRN1 as Modbus TCP/IP slave


Note: Only DTM for serial communication (ZBRN2) can be used in SoMachine V4.1 - Modbus TCP is not possible that time with SoMachine v4.1 (ZBRN1)!
Today if we check with SoMachine version v4.3, we can add ZBRN1 as Modbus TCP/IP Server

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: