{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What can cause an EEF1 control EEPROM fault on the ATV61 and ATV71 drives?

Issue:
EEF1 control eeprom fault on an Altivar ATV61 ATV71

Product Line:
Altivar drives ATV61 and ATV71

Environment:
All

Cause:
Internal memory fault on the control board.

Resolution:
EEF1= Control EEPROM fault.
Save a copy of the program in the keypad display 1st
Try resetting the drive back to a factory default to see if the fault will clear.
If the fault does not clear you will need get the drive repaired or try to replace the main control board.

Schneider Electric Nigeria