Issue:
Are line reactor required on the Schneider Electric Soft starters?
Product Line:
ATS22, ATS48, ATS46, ATS01, ATS23
Environment:
All
Cause:
Will the Schneider Electric ATS soft starters required any filtering or line conditioning device up stream.
Resolution:
No, the Schneider soft starters do not required any filtering or conditioners up stream. Soft starters only ramps up the voltage with very little harmonic distortion.
Released for:Schneider Electric Nigeria