{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the ATS22 adjustment range for parameter In, Motor Rated Current?

Issue:
Motor Rated Current adjustment range on the ATS22.

Product Line:
Altistart 22 ATS22

Environment:
All models

Cause:
What range of motors can be used for a particular ATS22 model

Resolution:
The Motor Rated Current, In, is adjustable from .4x to 1.0x the ATS22 current rating, IcL.
In other words, it can be adjusted down to 40% of the ATS22's rating.

Eg: An ATS22C17S6U, rated 170A, has an In range of 68 - 170A.

Schneider Electric Nigeria