{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do you program the customer enclosed drive to follow speed pot in hand and auto modes?

Issue:
Programming drive to follow the speed por in hand and auto modes.

Product Line:
M-flex, E-flex etc

Environment:
All

Cause:
They do not have a separate 4- 20mA speed signal for auto mode so they want to use the speed pot mounted on the enclosure in auto mode.

Resolution:
Programming changes as follows
Main menu
Set access level to Expert

Drives menu
Menu 1.6
Ref 1 - AI1
Ref 2 switching is channel 1 active

Menu 1.7
Ref switching LI3
Ref 1b switching is AI1

Schneider Electric Nigeria