{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are possible causes for a SCF fault code on an ATV58?

Issue:
SCF is a Short Circuit Fault

Product Line:
ATV58, FLEX58

Environment:
All models and serial numbers

Cause:
Possible causes are:
1.  heat sink fans are not operating
2.  The output transistors (IGBT) are not gating correctly
3.  Short circuit in the motor or motor wiring
4.  capacitance due to long motor lengths

Resolution:
1.   replace the heat sink fans
2.   repair or replace the drive.  This drive has been discontinued.  Parts may not be available.
3.   check motor for shorts,  Megger motor and motor wires with minimum of 1000v megger
4.   add a load filter

Schneider Electric Nigeria