{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where is the working folder for my Vijeo Designer V6.2 project files?

Article available in these languages: Spanish

Issue:
Looking for the directory on my PC where the Vijeo Designer 6.2 project files are located.

Product Line:
Vijeo Designer 6.2

Resolution:
The default path for the Vijeo Designer V6.2 projects can be found at the following locations
NOTE: This folder is only for the working folder of your project. It contains all the raw data of your application and should not be modified or altered outside of Vijeo Designer. If you wish to archive your project, please Export a VDZ file from within Vijeo Designer. Close the application first, right-click on it, and then choose "Export". The dialog will allow you to create a VDZ file to store anywhere you choose.

For Windows 7, Windows 10 users:
C:\Users\Public\Documents\Vijeo-Designer 6.2\Vijeo-Manager

For Windows XP users:
C:\Documents and Settings\All Users\Documents\Vijeo-Designer 6.2\Vijeo-Manager

This default path can only changed during the the installation of the software.

Schneider Electric Nigeria