Issue:
What materials are used in the Magelis XBTGT6330/GT6340 housing?
Product Line:
XBTGT6330, XBTGT6340, XBTGT
Environment:
Physical Human Machine Interface (HMI)
Resolution:
Below are the materials used in the Magelis XBTGT6330/GT6340 targets:
Below are the materials used in the Magelis XBTGT6330/GT6340 targets:
Part Name Material Flame Resistance
Front Sheet PET UL94 VTM-2
Front Bezel ADC12
Rear Cover PC/PBT UL94 V-0
Released for:Schneider Electric Nigeria