Product Line:
All ATV61/71
Environment:
All environments
Cause:
Fixing a JOG speed or configuring a JOG input.
Resolution:
The jog function allows the user to run at preset speed equal to or less than 10hz when an assigned input is activated.
Jog function assignment can be found in the Application Function Menu.
To configure the JOG :
[1.7 APPLICATION FUNCT.]
[JOG]
"JOG" select the input
"JGF" select JOG speed
Released for:Schneider Electric Nigeria