{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the Altivar ATV312 drive be used as a phase converter?

Issue:
Can the ATV312 be used as a phase converter?

Product Line:
Altivar 312 for single phase line power

Environment:
VFD for single phase line power

Cause:
VFDs to be used as phase converters, to convert single phase line power to 3 phase line power.

Resolution:
Schneider offers the ATV312 that can be used to convert single phase line power to 3 phase output.  For selection: see the ATV312 quick start annex link below.
https://www.se.com/us/en/download/document/S1B16328/

Using a drive as a phase converter is possible only for motors. DO NOT USE DRIVES FOR PHASE CONVERTER FOR MACHINES.
The "input phase loss detection" must be deactivated (IPL=no)

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.