{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PowerLogic EM4800 Series Meter Brochure
Issue
A user requires to view specifications, features, and capability of all models within PowerLogic EM4800 Series meters.
Product Line
EM4800, EM4805, EM4833, EM4880
Environment
Feature and Capability, Comparison Table, Technical Datasheet, Brochure
Cause
A user would like to View and Compare Technical Specification of EM4800 Series meters to select the appropriate PowerLogic EM4800 Model.
Resolution
There are two attachments for the Brochure and Technical Datasheet.
See attached documents:

Schneider Electric Nigeria

Attachment(s)
EM4800_Multi_Circuit_Energy_Meter_Brochure.pdf [1.19 MB]
PowerLogic_EM4800_Series_Technical_datasheet.pdf [1.17 MB]