{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why is the numeric display object input ranges are 0 for the min and max in Vijeo Designer simulator and runtime?
Issue
In Vijeo Designer Simulation Mode or Runtime, why are the Numeric Display object input ranges shown as 0 for the Min and Max in the Numeric Value Entry keypad?

Product Line
Vijeo Designer

Environment
HMI Runtime and HMI Simulation Mode

Cause
If the variable is a Real (Floating Point) and the Numeric Display object was setup as an Integer data type, the Min and Max will appear as 0.

Resolution
Change the Data Type radio selector in the Numeric Display object from "Integer" to "Float" to represent the "Real" Data Type of the actual Variable.

Schneider Electric Nigeria