{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can I use circuit breakers other than those published in the Quick Start Annex Guide S1A14738 to achieve the same short circuit current ratings?

Issue:
Is it ok to use circuit breakers other than those published in the Quick start guide S1A14738 in order to achieve the same short circuit current ratings?

Product Line:
ATS22

Environment:
All models and serial numbers of ATS22

Cause:
None

Resolution:
Only those circuit breakers published in document S1A14738 Quick start guide - Altistart 22 ANNEX for UL 508 market can be used to achieve the short circuit current ratings listed.

Schneider Electric Nigeria