{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does drive output voltage follow the output frequency?

Article available in these languages: Spanish

Issue:
Drive output voltage appears to follow the output frequency.

Product Line:
Altivar

Environment:
All

Cause:
Output of drive at low speed was lower than the mains voltage

Resolution:
Yes, the drive output voltage can be controlled with drive frequency.
Drives are usually supplied with AC power. The power that comes in to a controller is at a set frequency.
The motor controller first turns that AC to DC, then turns the DC back into AC at the right frequency.
The speed of any AC motor is dependent on the applied frequency.

Schneider Electric Nigeria