{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the TM2 I/O modules be used on a M221 controller?
Issue:
Using TM2 modules with the M221

Product line:
TM221

Environment:
EcoStruxure Machine Expert Basic (formally SoMachine Basic)

Cause:
Twido obsolete and replacement is the M221

Resolution:
Yes, but the TM2 modules have to be mounted after any TM3 modules if TM3 modules are used.

Schneider Electric Nigeria

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.