{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to Restore Backup Database from SQL 2005 to SQL 2012
Issue: 
When trying to restore a SQL 2005 database in SQL 2012, the Database Restore will give the following error: “The database was backed up on a sever running version 8.002065. That version is incompatible with this server, which is running version 11.00.3000.”
 
Product Line: 
Power Monitoring Expert v7.2.2
 
Environment: 
SQL Server Management Studio
 
Cause: 
It is not possible to restore a SQL 2005 database directly to SQL 2012. 
 
Resolution:
1) Restore the SQL 2005 database backup on a SQL Server 2008 system. 
2) Take a backup of the database from the SQL 2008 system. 
3) Restore the SQL 2008 database backup on the SQL 2012 system. 

Schneider Electric Nigeria

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.