{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can I hot swap a CPS1xx xx Power Supply?
Issue:

No, the 140CPS110 00 cannot be hot swapped when supporting a CPU. Doing so will interrupt the CPS hold up time which the CPU will need in order to back up the program.


Product Line: Quantum


Environment:n/a


Cause:n/a


Resolution:n/a


R-101317

Schneider Electric Nigeria