{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What will cause the ATV212 drive not to start when the run contact between P24-F is closed?
Issue:
The ATV212 drive does not to start when the run contact between P24-F is closed.

Product Line:
Altivar ATV21 and ATV212

Environment:
All

Cause:
When closing the run contact to logic input F, the VFD displays 0.0Hz.

Resolution:
- Verify that CMOd is set to 0 for terminal control.
- If any network functions are activated for monitoring purposes, set F108 = 48.
- Check your logic input programming.  Typically F111 = 2 for run forward function.  Other possibilities may combine run forward with other functions.
- Verify that the VFD is in Remote Mode.  The keypad LOC/REM button green LED should be OFF.
- Verify the VFD 24Vdc power supply by measuring P24 - CC.
- Check that the run circuit is complete by measuring for 24Vdc on F - CC.
- Verify that the VFD has a speed reference.  It may be running at 0Hz, indicated by a red RUN LED in the display.
- Verify whether the run permissive is being satisfied. If the drive displays "OFF", then the run permissive isn't satisfied. However, "OFF" is a normal state if the run permissive is activated when the run command is given.

Schneider Electric Nigeria

Attachment(s)
atv212_programming_manual_en_s1a53838_02.pdf [3.58 MB]