{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How to ping multiple IP address in a range of IP address

Article available in these languages: Czech

Issue
User wants to ping multiple IP address

Product
Any requiring communication with IP address

Environment
Command Prompt

Cause
User wants to ping multiple IP address with one command

Resolution
Run the following command
for /L %z in (1,1,254) do @ping 10.0.0.%z -w 10 -n 1 | find "Reply"

Change the IP address after the ping command to reflect your networks IP range. The above command will ping each address between 10.0.0.1 and 10.0.0.254 and return the IP address that replay to the ping

edit: The -w 10 makes it only wait 10 ms for a reply before moving on. If your network is slow you will have to up this value or take it out all together.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.