{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How much separation is required between communications cables and power cords?

Issue:
There is a concern that power cords can interfere with signal integrity in data cables if they're installed too closely.

Product Line:
NetShelter SX, NetShelter SV, NetShelter VX, NetShelter WX

Environment:
All versions and serial ranges.

Cause:
Data cables and power cords are sometimes installed in close proximity or may overlap.

Resolution:

The ANSI/TIA-569-C standard speaks directly to the separation of telecommunications and power cables. The recommended distance can vary. Please see ANSI/TIA-569-C.
Anixter has posted a document titled *Anixter Standard Reference Guide that includes excerpts from ANSI/TIA-569-C. In this guide, pages 67 - 68 speak specifically to this question: https://www.anixter.com/en_us/resources/literature/technical-references/standards-reference-guide.html

Besides the ANSI/TIA-569-C, this guide includes information from the following standards: ANSI/TIA-568-C.0, ANSI/TIA-568-C.1, ANSI/TIA-568-C.2, ANSI/TIA-568-C.3, ANSI/TIA-606-B, ANSI/TIA-607-B, ANSI/TIA-862-A, ANSI/TIA-942-A, ANSI/TIA-1005, ANSI/TIA-1179, ISO/IEC 11801, ISO/IEC 11801 Class Ea, IEEE 802.3af, IEEE 802.3at, IEEE 802.3an, IEEE 802.3ba and IEEE 802.1.

*This document is not intended to be a substitute for the original standards documents. For a complete copy of any topic in the Guide, please refer to the original standards documents. There is a section in this guide "Reference Documents" where you will find instructions on how to order a current copy of these standards.


Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: