{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
When using the HMI for speed control on the ATV61 or ATV71 drives can the drive run faster than the programmed high speed settings?
Issue:
Operating the drive in Local mode, the dial allows the speed reference to be adjusted above the 60Hz of High Speed value.

Product Line:
ATV71 Altivar 71

Environment:
All ATV61 and ATV71 drives

Cause:
Installation / Setup

Resolution:
The drive will not operate faster than the programmed high speed.  The HMI reference can be adjusted above the high speed parameter, but the drive will not actually operate beyond the high speed setting.

Schneider Electric Nigeria