{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What should parameter bFr be set to if you are using a 50hz 400vac motor?
Issue:
Setting up bFr parameter for a 50hz 400vac motor.

Product Line:
ALTIVAR ATV61

Environment:
All

Cause:
Installation / Setup

Resolution:
Drive settings for bFr, nPr, UnS , nCr and nSP settings,  should match the motor nameplate.
in this case bFr will be set to 50hz and UnS will be set to 400vac

Schneider Electric Nigeria

Attachment(s)
atv61_programming_manual_en_1760649_08.pdf [4.35 MB]