{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is Concept software supported on Windows 7 Professional (64 bit) operating systems?

Issue:
Can Concept be installed on a Windows 7 64 bit OS.

Product line:
Concept Software and all supported PLC's.

Environment:
Concept 2.6 sr7

Resolution:
Concept is not supported on Windows 7 Professional (64 bit) operating systems.
Concept 2.6 SR7 has been validated and will run on  Windows 7 Professional (32 bit) operating systems. This was the last release version of concept with service patches no further updates will be provided.

NOTE: Concept is obsolete and has been replaced with Ecostruxure Control Expert (formally Unity Pro). All hardware that is supported with Concept is also obsolete and it is recommended to upgrade obsolete hardware with appropriate current hardware.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: