{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ION8600 and ION8650 meter shows message "CONFIGURATION MODE LOCKED OUT" on front panel
Issue
ION8600 and ION8650 meter shows message "CONFIGURATION MODE LOCKED OUT" on front panel

Product Line
ION8600, ION8650

Cause
Upon attempt to view or configure meter from the front panel by holding down the ALT/ENTER key, the message "INFORMATION CONFIGURATION MODE LOCKED OUT" appears and holds on the screen until timing out.

Environment
Configuring ION8600/8650 via the front panel.

RESOLUTION
Configuring ION8600/8650 via the front panel has been set to be disallowed. Access the meter via communications using ION Setup or ION Designer. Find the Display Options module and change the setting of the setup register called "Front Panel Programming" to "Allowed".

Schneider Electric Nigeria