{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to setup a PTC alarm without tripping the ATV61 drive?

Article available in these languages: Spanish

Issue:
PTC alarm installation

Product Line:
Altivar 61, Altivar 71

Environment:
All models, all serial numbers

Cause:
Using PTC probes for motor overload protection, requesting warning indication rather than faulting the VFD

Resolution:
PTC warning can be indicated via a relay output assigned to an Alarm Group.
Example for SW2 switch set to PTC, PTC connected to LI6, R2 indication, Alarm Group 1

1.8 Fault Management
PTC Management - activates the PTC monitoring
LI6 = PTC Probe [PTCL] = Always

Motor Thermal Prot - Inactivates the VFD internal I2T overload protection
Overload Fault Mgt [OLL] = Ignore

1.5 Inputs/Outputs CFG
R2 Configuration - assign relay R2
R2 Assignment [R2] = Alarm Grp1

Alarm Grp1 Definition - activate PTC alarm for the warning group
LI6 = PTC Alarm [PLA] = ON

Important note:  When Overload Fault Mgt [OLL] = Ignore, the motor thermal protection by calculating the I2t is inactive.  The drive will not provide motor overload protection based on motor current.  Both functions can work at the same time by keeping Overload Fault Mgt [OLL] = Freewheel

Schneider Electric Nigeria

Attachment(s)
atv61_programming_manual_en_1760649_08.pdf [4.35 MB]