{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Does Schneider Electric have an 8 pole isolator in its portfolio?

When it is referred to 6-pole/8-pole isolator or switch-disconnector, usually what is meant is a set of changeover assembly (2x3P/2x4P). Check the attached image as an example of an 8-pole switch-disconnector (refer to 8 Pole switch-disconnector.png). So upon the rating, you could be directed to the suitable switch-disconnector assembly. For example, for 8P 250A rated isolator, you would be advised to use the attached order form (Compact INS or Compact NSX)

Schneider Electric Nigeria

Attachment(s)

8 Pole switch-disconnector.png8 Pole switch-disconnector.png [67.16 KB]
Order form - Source Changeover Systems.pdfOrder form - Source Changeover Systems.pdf [273.99 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: