Search FAQs
How can you identify if the ATV61/71 drives are Fuji built drives when ordering replacement parts?
Issue:
Identify if the ATV61/71 drives are fuji built drives when ordering replacement parts.
Product Line:
Altivar ATV61 and 71 frame sizes 9 thru 15 230 vac and 460 vac.
Environment:
All
Cause:
Needs to identify if the drive in question has MItsubishi or Fuji built IGBTs, Power Boards, Measurement boards and Gate driver boards.
Resolution.
Get the serial number of the drive and locate the 8th digit (counting from left to right) to see if its a 2 which tells you that the drive has Fuji built parts.
Example: Serial number is 6W09470(2)1001
If the 8th digit is 2= Fuji modules
If the 8th digit is 0=Mitsubishi modules
If the 8th digit is 5=Mitsubishi modules
Note that any serial number beginning with EL was built with Mitsubishi components.
The Fuji modules will have a F suffix on the end of the part number.
Identify if the ATV61/71 drives are fuji built drives when ordering replacement parts.
Product Line:
Altivar ATV61 and 71 frame sizes 9 thru 15 230 vac and 460 vac.
Environment:
All
Cause:
Needs to identify if the drive in question has MItsubishi or Fuji built IGBTs, Power Boards, Measurement boards and Gate driver boards.
Resolution.
Get the serial number of the drive and locate the 8th digit (counting from left to right) to see if its a 2 which tells you that the drive has Fuji built parts.
Example: Serial number is 6W09470(2)1001
If the 8th digit is 2= Fuji modules
If the 8th digit is 0=Mitsubishi modules
If the 8th digit is 5=Mitsubishi modules
Note that any serial number beginning with EL was built with Mitsubishi components.
The Fuji modules will have a F suffix on the end of the part number.
Released for:Schneider Electric Nigeria
Attachment(s)
Explore more
Range:
Explore more
Range: