Issue:
Need to size a full voltage bypass contactor for the open type ATS48 soft starters.
Product Line:
Altistart ATS48
Environment:
All
Cause:
Needs to add a full voltage bypass contactor to an open type ATS48 soft starter.
Resolution:
You will size the full voltage bypass contact to the size of the motor amps. Please note that if you field install a bypass contactor you may need to add a line isolation contactor and add NC contacts so that you can turn off the soft starters control CL1 CL2 control voltage when you are in full voltage bypass.
Need to size a full voltage bypass contactor for the open type ATS48 soft starters.
Product Line:
Altistart ATS48
Environment:
All
Cause:
Needs to add a full voltage bypass contactor to an open type ATS48 soft starter.
Resolution:
You will size the full voltage bypass contact to the size of the motor amps. Please note that if you field install a bypass contactor you may need to add a line isolation contactor and add NC contacts so that you can turn off the soft starters control CL1 CL2 control voltage when you are in full voltage bypass.
Released for:Schneider Electric Nigeria