{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to identify and update outdated Statistics in SQL Server

Issue
A user may be experiencing performance issues when running SQL queries.

Product Line

Power Monitoring Expert 7.2.x

Power Monitoring Expert 8.x

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023



Environment
Power Monitoring Expert Software with either SQL Server Versions (2005- 2022)

Cause
Outdated statistics can make the SQL server choose a non-optimal execution plan causing undesirable slow response times for certain queries.

Resolution
*Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio. Databases should be backed up prior to performing this procedure.*

To identify tables within the database which have outdated statistics, the following query can be used.


SELECT OBJECT_NAME(id) AS Table_Name, st.[name] AS Tname, si.name,
STATS_DATE(id, indid) AS DateLastUpdate,rowmodctr rowsModifiedSinceLastUpdate
FROM sys.sysindexes AS si
INNER JOIN sys.[tables] AS st ON si.[id] = st.[object_id]
INNER JOIN sys.schemas AS ss ON st.[schema_id] = [ss].[schema_id]
WHERE STATS_DATE(id, indid)<=DATEADD(DAY,-1,GETDATE())
AND rowmodctr>10
ORDER BY[rowmodctr] DESC


Once you have identified tables with outdated statistics, the UPDATE STATISTICS  statement can be used to
bring the statistics back up to date.
UPDATE STATISTICS Table_Name

Schneider Electric Nigeria

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: