{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What it he maximum number of SoMachine protocol connections for a TM241 and TM251 controller?
There is a maximum of eight SoMachine protocol connections for the embedded Ethernet port of a TM241 or TM251 controller. SoMachine will use one of these connections to connect to the PLC.
This information is for controllers with a firmware version corresponding to SoMachine v4.3.

Schneider Electric Nigeria