{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the part number for the M580 weighing module?

Issue:
Part number for the M580 weighing module


Product Line:
M580


Resolution:
The part number for the M580 weighing module is PMESWT0100. Itis a versatile and flexible weighing module controller, which can be used wherever weighing scales are to be used in the Schneider Electric Modicon X80 automation system.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: