Issue:
Is ATV212 S-Flex available in a Nema 4 or 4X enclosure?
Product Line:
ATV212 S-Flex, all models
Environment:
ATV212 in S-Flex, all models
Cause:
Does SFLEX-212 come in a Nema 4 or 4X enclosure?
Resolution:
No, the ATV212 S-Flex is available in a Type 1, Type 12, and Type 3R enclosures, but there is no option for a Nema 4 or 4X version.
See the S-Flex manual for details : https://www.se.com/us/en/download/document/30072-451-83/
For other enclosed drive options, please look at our ATV660, ATV960, Altivar Outdoor Drive or custom-built drive panels.
Is ATV212 S-Flex available in a Nema 4 or 4X enclosure?
Product Line:
ATV212 S-Flex, all models
Environment:
ATV212 in S-Flex, all models
Cause:
Does SFLEX-212 come in a Nema 4 or 4X enclosure?
Resolution:
No, the ATV212 S-Flex is available in a Type 1, Type 12, and Type 3R enclosures, but there is no option for a Nema 4 or 4X version.
See the S-Flex manual for details : https://www.se.com/us/en/download/document/30072-451-83/
For other enclosed drive options, please look at our ATV660, ATV960, Altivar Outdoor Drive or custom-built drive panels.
Released for:Schneider Electric Nigeria