Issue:
Needs the part numbers of the measuring board for the ATV61HC16N4 and ATV71HC13N4 drives
Product Line:
ATV61 and ATV71
Environment:
All
Cause:
Failed measuring board component within the drive.
Resolution:
The part number for the measuring board is VX5A71HC13N4 or VX5A71HC13N4F (For Fuji parts)
When a replacement Measurement board is needed, the serial number of the VFD needs to be verified.
If the 8th digit of the Serial number is a "2" as shown below than the replacement part number must have an "F" suffix.
See Attachment
Released for:Schneider Electric Nigeria